programming flash device, MPC 8548, CW8.7, IDE 5.9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

programming flash device, MPC 8548, CW8.7, IDE 5.9

3,703 Views
sai
Contributor I
We have a spansion flash device S29GL256P. Using CodeWarrior I'm trying to program that flash device. The closest device I found in the list of devices is S29GL256N. I tried selecting this device but it didn't work. It says "Initializing..........." and stays there forever.

* Is there a version of CodeWarrior that supports the S29GL256P flash device.

* Is it possible to use any device in the existing list of devices to be able to program the S29GL256P flash device.

Thanks
-Sai
Labels (1)
0 Kudos
Reply
2 Replies

1,661 Views
tkvenki
Contributor III

Hi sai,

 

 I have the same issue, which you are facing.

Let me know if you get any lead on this.

 

Also,

 Freescale has provided some guide which will tell how to create our own FLASH device.

 

http://www.freescale.com/files/soft_dev_tools/doc/white_paper/CWFLASHPROWP.pdf

 

The above link may help you to go ahead.

 

I will le you know if I take this up...

 

0 Kudos
Reply

1,661 Views
Voxan
Contributor III
Hi there,

I would recommend to request this support to the support team at

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=05

click on the 'request help (online)' link.

Regards

0 Kudos
Reply