no BSP code after installing BSP/ltib package?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no BSP code after installing BSP/ltib package?

1,815 Views
KurtZou
Contributor I

Hi all,

I've downloaded MPC85xx BSP/ltib package from this site. After intall ,there's no BSP code?where can I find that:robotvery-happy:

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,013 Views
KurtZou
Contributor I

Thanks genuap! this really helps.

One more question, where's u-boot source code? I think source under ..../rpm/BUILD/linux is kernel code right?

0 Kudos
Reply

1,013 Views
genuap
NXP Employee
NXP Employee

After you install the ltib, you need to go into the installation directory and configure it - run the ltib GUI:

 

./ltib -c

 

Then you can select which packages you want, what you want in the kernel etc... This'll take a while - because it has to extract all of the packages, and compiles them. When it's done, you can find the source in:

 /ltib_intsll/rpm/BUILD/linux/

 

 

0 Kudos
Reply