modifying the SRAM _init.tcl file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

modifying the SRAM _init.tcl file

ソリューションへジャンプ
1,504件の閲覧回数
jagxin
Contributor III

Dear all ,

                How to modify the sram _init file of P2041 for adding a FRAM connected to CS2 of p2041  in the hardware 

103300_103300.pngpastedImage_0.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,328件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello agxin j,

You'll need to add this part for CS2 into eLBC controller setup section,  you could refer to and edit base on the part for CS0:

    # eLBC_BR0

    mem [CCSR 0x124000] = 0xe8001001

    # eLBC_ORg0

    mem [CCSR 0x124004] = 0xf8000f85

eLBC_BR1 is for setting base address, port size, machine select and so on. Change the CCSR address from 0x124000 to 0x124008.

eLBC_ORg1 is mainly for setting address mask. Change the CCSR address from 0x124004 to 0x12400C.

Both the two registers are defined in chip reference manual, refer it for details field descriptions.

And add the part for the memory on CS2 in the LAW setup section,  refer to and edit base on the part for CS0:

  mem [CCSR 0xc00] = 0x00000000

    mem [CCSR 0xc04] = 0xE0000000

    mem [CCSR 0xc08] = 0x81f0001b

This is for the memory map of the adding memory. Change the CCSR address to be the windows registers chosen, 0xCn0, 0xCn4, 0xCn8. The three registers could also be found in chip reference manual, refer to Section 2.4.

Finally add the MMU initialization for it, also refer to and edit base on the part for CS0:

reg ${CAM_GROUP}L2MMU_CAM2  = 0x9000000A1C080000E0000000E0000001Detail description of this register is contained in doc Targeting_PA_Processors.pdf, the doc is located in: D:\Freescale\CW_PA_v10.5.0\PA\Help\PDF


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,329件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello agxin j,

You'll need to add this part for CS2 into eLBC controller setup section,  you could refer to and edit base on the part for CS0:

    # eLBC_BR0

    mem [CCSR 0x124000] = 0xe8001001

    # eLBC_ORg0

    mem [CCSR 0x124004] = 0xf8000f85

eLBC_BR1 is for setting base address, port size, machine select and so on. Change the CCSR address from 0x124000 to 0x124008.

eLBC_ORg1 is mainly for setting address mask. Change the CCSR address from 0x124004 to 0x12400C.

Both the two registers are defined in chip reference manual, refer it for details field descriptions.

And add the part for the memory on CS2 in the LAW setup section,  refer to and edit base on the part for CS0:

  mem [CCSR 0xc00] = 0x00000000

    mem [CCSR 0xc04] = 0xE0000000

    mem [CCSR 0xc08] = 0x81f0001b

This is for the memory map of the adding memory. Change the CCSR address to be the windows registers chosen, 0xCn0, 0xCn4, 0xCn8. The three registers could also be found in chip reference manual, refer to Section 2.4.

Finally add the MMU initialization for it, also refer to and edit base on the part for CS0:

reg ${CAM_GROUP}L2MMU_CAM2  = 0x9000000A1C080000E0000000E0000001Detail description of this register is contained in doc Targeting_PA_Processors.pdf, the doc is located in: D:\Freescale\CW_PA_v10.5.0\PA\Help\PDF


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信