how to loading and run binary image under codewarrior with mcf52254

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to loading and run binary image under codewarrior with mcf52254

跳至解决方案
3,582 次查看
robert_zhang
Contributor I

1.i check the 'generate binary image' on setting window.

2.in flash programmer, i select program/verify ,check 'used selected file' and select binary file that have already generated.

3.click 'erase','program' button, it display successful.

4.but when i reset the target board, there was nothing in uart.

i used to download elf type file into 52254, it will run ok and will display welcome message through uart.

who can help me and tell me how to right set other config to keep it run normally?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,946 次查看
MCF52233
Contributor III

Hi Robert,

i really dont knw what exactly problem with codewarrior to generate bin file. But i'm sure there is some decrepency in data,rather than u can try S19 to bin file converter which will work for u.

chk tunercat.com for s19 to bin converter

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,947 次查看
MCF52233
Contributor III

Hi Robert,

i really dont knw what exactly problem with codewarrior to generate bin file. But i'm sure there is some decrepency in data,rather than u can try S19 to bin file converter which will work for u.

chk tunercat.com for s19 to bin converter

0 项奖励
回复
1,947 次查看
robert_zhang
Contributor I
under you tip, i have check help system on flash binary file again, i found the binary file that the codewarrior generated was a binary version of s-record, but the flash programmer only process raw binary file.the size of my code was small,and the mcu chip has too much flash to use, so i decided to give up this idea.
0 项奖励
回复
1,947 次查看
gmnelson
Contributor III

I'm having this problem right now.  We've written code to download (via the web browser) a raw binary image file and store it in a Serial SPI flash device.  Unfortunately we have realized the 'binary image' generated by CodeWarrior is not a 'RAW' binary image - it's a binary version of the .s19 file.

 

What's up with this?  Who uses a binary image of the s19 file???

0 项奖励
回复