fp_coldfire.a rebuild for register parameter passing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fp_coldfire.a rebuild for register parameter passing

3,342件の閲覧回数
jjr
Contributor I
Hi, we're using CW 6.3 and have imported the libray "CodeWarrior for ColdFire V6.3\E68K_Support\Libraries\fp_coldfire.a"  into our project for floating point.Originally the project was built
using stack parameter pasing. We want to change it to use register passing. What
project in the "CodeWarrior for ColdFire V6.3\E68K_Support\*" tree must I rebuild to do this ?
 
 Thanks,
 John
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,170件の閲覧回数
tim35ca
Contributor I
There doesn't seen to be a RegABI version of the library fp_coldfire.a or a way to build it.
0 件の賞賛
返信

1,170件の閲覧回数
CrasyCat
Specialist III
Hello

fp_coldfire.a contains only functions implemented in assembly language.
There is no parameter passing scheme for assembly functions, so there is no need to have RegABI version of these library.

Also functions from this library are used internally by the compiler. They should never be used by the programmer.

CrasyCat
0 件の賞賛
返信

1,170件の閲覧回数
CrasyCat
Specialist III
Hello
 
Please look at {Install}\Help\PDF\ColdFire_Build_Tools_Reference.pdf.
Chapter "ColdFire Runtime Libraries", section "MSL for ColdFire Development" -> "Using MSL Libraries for ColdFire" includes a table showing naming convention for MSL & Runtime libraries.
 
RegABI_ is the substring you need to look for for register ABI.
 
CrasyCat
0 件の賞賛
返信