debugger interface for M5211DEMO board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

debugger interface for M5211DEMO board

1,642 Views
louiswang
Contributor I

I use CodeWarrior V7.1 special edition/M5211DEMO integrated USB-BDM interface for a project.

When I start a new project, which connection should I choose?

There are a number of  selections:

1)P&E USB BDM Multilink. 2) Parallel BDM Multilink. 3)Ethernet-TAP BDM.

4)Freescale USB-TAP BDM. 5),6),7)for licensed CodeWarrior.

8)P&E Cyclone Max.  9)TCP-IP cyclone max 10)serial cyclone max

11)P&E lightning

Thanks

 

L.W

Message Edited by louis wang on 2009-09-13 08:35 PM
Labels (1)
0 Kudos
Reply
1 Reply

960 Views
pgo
Senior Contributor V

Dear Louis,

 

According to the Demo board manual

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=M5211DEMO&fpsp=1&tab=Documentation_Ta...

 

The BDM is an integrated P&E debugger

 

So choose the 1) option.

 

There should be a Quick-start document with the board that explains this.  I couldn't find it online unfortunately.

 

bye

 

Message Edited by pgo on 2009-09-14 04:24 PM
0 Kudos
Reply