console debug problem for CW for Coldfire 6.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

console debug problem for CW for Coldfire 6.3

2,156件の閲覧回数
perfume
Contributor I

Hi, I'm using Codewarrior for Coldfire architectures, v6.3, targeting a M52233DEMO. I followed the quick start instruction's setting and example to build and run the example project,  when doing console debug, a window appears which says: unable to use the plugin"CCS_CF_Protocol_Plugin". It is licensed and a valid license key was found. CFCCSProtocolplugin: Can't connect to CCS. But when I  do UART debug, it works. How to solve this console debug problem. Thanks so much


J2MEJediMaster added CW type and version to subject line


Message Edited by J2MEJediMaster on 2007-06-07 10:14 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

957件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Which target connection/remote connection are you using?

The remote connection to be used can be confiured in the settings on a per build target basis, so the Console Debug may be configured for CCS (say to connect to a FSL USBTab) while the others may connect using another remote connection.

Daniel
0 件の賞賛
返信