connecting to code warrior usb tap - help needed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

connecting to code warrior usb tap - help needed

3,917 Views
Amihay
Contributor I

Can anyone help me or send me a link to a document that describe how to configure and connect to the usb tap. I am using codewarrior IDE ver 5.9.0 build 2521.

 

Thanks 

Labels (1)
0 Kudos
Reply
4 Replies

2,319 Views
CrasyCat
Specialist III

Hello

 

- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.

 

CrasyCat

0 Kudos
Reply

2,319 Views
Amihay
Contributor I

Hi,

 

I am using codewarrior IDE version 5.9.0.

using ppc8360 with e300c1 core.

I am using windows XP professional on my laptop  

 

anyway, I succeeded to connect to the tap but I am facing new problems:

1. I am looking for an example suitable for ppc8360.

2. when trying loading an example to the board, I get the following message: "please check your JTAG clock speed"

3. what is the suitable .cfg script that I should use?

 

Thanks,

Amihay 

0 Kudos
Reply

2,319 Views
ronco
NXP Employee
NXP Employee

Hi Amihay,

 

The "please check your JTAG clock speed" error tells me that you need to update your CodeWarrior for Power Arch software.  The IDE version 5.9.0 doesn't tell you the version of CodeWarrior you have, only the IDE version. Do this: In the CodeWarrior IDE go to Help->About->Installed Products and you'll see your CodeWarrior version.  If it's less than 8.8 CW PA you'll need to download and install the 8.8 CodeWarrior PA software followed by the 8.8.3 CW PA Update.  I hope this helps.

 

-Ron

0 Kudos
Reply

2,319 Views
robert_zhang
Contributor I

do you have see the 'usb tap users guide'?it maybe helpful to you.

you also can search 'usb tap' in 'Enter Keyword' in editbox at right-up on freescale homepage.

there will list some of documents about usb-tap.

0 Kudos
Reply