code warrior v8.7 for Power PC installation issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code warrior v8.7 for Power PC installation issue

4,760 Views
cgc056
Contributor I
hi,
 
I try to install code warrior v8.7 for powerpc family, but at the end of installation before it is all completed, I get a WDREG error, indicate 2 applications are using the WinDriver, i must quit out of the applications or cancle the installation and reboot.  I have tried exit all of the application that I am aware of it,  also try to reboot and reinstall again, but I always get the same error message at the same point.  Does anyone out there ever experience the same problem?  Or how can I find an application that is using the WinDriver?  I will appreciate any comments and feedback on this one.
 
Thanks!
 
cgc045
Labels (1)
0 Kudos
Reply
4 Replies

2,663 Views
genuap
NXP Employee
NXP Employee
Do you have the WindRiver tools installed as well (or another vendor's)? I've seen issues with this. Either uninstall WindRiver's tool, or you should be able to see some processes relating to WindRiver in the process list - kill them and the install should go through.

Is should be something like Windriver or Win something - If I can find my visionclick machine I'll let you know for sure.

 ... Paul

0 Kudos
Reply

2,663 Views
cgc056
Contributor I
what don't I have from WindRiver.  I actually have several version of visionclick, workbench installed on my pc.  But I took your suggestions and killed every windriver tool related process and then i was able to install the code warrior!  Thanks for your help, Paul!
 
cgc056
0 Kudos
Reply

2,663 Views
CrasyCat
Specialist III
Hello
 
Can you try to remove all HTI connected to your Host PC before you install the CodeWarrior software.
All interface cables (USBTAP, ...)  connected through either USB or parallel port should be disconnected from the host before you install the tools.
 
You should get rid of the message then.
 
CrasyCat
0 Kudos
Reply

2,663 Views
cgc056
Contributor I
thanks for the reply.  I disconnect all extenal devices and cables on the usb, serial and parelle port.  but I am still getting the same WinDriver (WDREG) error.  any other suggestions?
0 Kudos
Reply