Writing driver codes on Yocto's layer or creating a higher level layer that includes meta-ppc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Writing driver codes on Yocto's layer or creating a higher level layer that includes meta-ppc

1,533件の閲覧回数
cengizhanyapici
Contributor I

In my Yocto project,I want to implement my driver codes to Yocto's layer.I use T1024rdbfor this purpose which has power pc architecture.So,in Yocto I think that meta-ppc layer is suitable for this purpose;on the other hand,creating a higher level layer which includes meta-ppc can give me the advantage of using also meta-ppc layer's properties.So,is it possible to create a new higher level layer which includes this meta-ppc layer or any documents,references or manuals about this topic?or could you recommend something about this issue?

Thanks for your answers.

Best Regards...

ラベル(1)
0 件の賞賛
返信
1 返信

1,332件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Cengizhan Yapicioglu,

For create a custom layer, you could refer to GitHub - yoctocookbook/meta-custom: Example meta-custom Yocto layer .

The attached is an example about how meta-freescale including dynamic-layers layer, please pay attention to meta-freescale_bak/conf/layer.conf configuration, especially BBFILES variable definition.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信