Windows XP CW for MPC55xx V2.2 flash programming error 14

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Windows XP CW for MPC55xx V2.2 flash programming error 14

2,594 次查看
PGB
Contributor I
Hi, every one!
What do the error code 14 means? Thanks!
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,285 次查看
peg
Senior Contributor IV
Hi,
Unfortunately the docs don't give any more information than you already have on the line above the error.
It tried to put the programming algorithm into the device and failed.

0 项奖励
回复

1,285 次查看
PGB
Contributor I
Thank you, peg!
I am using the CW for MPC55xx  with the board designed by me. I've checked every signal that I can. There's Vpp on 5.088V. The MPC5554 was configed as RSTCFG = 0, BOOTCFG=00, PLLCFG = 01, WKPCFG=1. The MPC5554 was clocked by a 16MHz oscillator (not by the crystal reference), and had no external memory (The extern bus interface connects nothing).
 
0 项奖励
回复