What is CCS chain_pos?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is CCS chain_pos?

ソリューションへジャンプ
2,542件の閲覧回数
kavitamathur
Contributor II

Hi,

 

I want to use following command on CCS prompt:

 

ccs::read_mem ::chain_pos ? address_hi? address size space count

 

My queries are :

 

1. What is chain_pos?

2. What is address_hi?

 

Please help me.

 

Thanks & Regards,

Kavita

ラベル(1)
0 件の賞賛
返信
1 解決策
2,295件の閲覧回数
hwrobel
NXP Employee
NXP Employee

Use the Debugger Shell to access memory. It is easier to use and supported.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,296件の閲覧回数
hwrobel
NXP Employee
NXP Employee

Use the Debugger Shell to access memory. It is easier to use and supported.

0 件の賞賛
返信
2,295件の閲覧回数
sinanakman
Senior Contributor III

Hi Heinz, how do you run the debugger shell ? is this part of CCS ?

This is the CCS I am running if the debugger shell is in another version  :

% show version

CCS Linux Release Build 365p0

CodeWarrior Connection Server version {4.13}

(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED

Thanks

Sinan Akman

0 件の賞賛
返信
2,295件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi,

You can open the debugger shell from CW: Window -> Show View -> Debugger Shell.

Marius

0 件の賞賛
返信
2,295件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi, Kavita

Yes, as Heinz said. You can use "mem" or "display" in debugger shell, type "help mem" or "help display" for detail description of command.

0 件の賞賛
返信