What is CCS chain_pos?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is CCS chain_pos?

跳至解决方案
1,855 次查看
kavitamathur
Contributor II

Hi,

 

I want to use following command on CCS prompt:

 

ccs::read_mem ::chain_pos ? address_hi? address size space count

 

My queries are :

 

1. What is chain_pos?

2. What is address_hi?

 

Please help me.

 

Thanks & Regards,

Kavita

标签 (1)
0 项奖励
回复
1 解答
1,608 次查看
hwrobel
NXP Employee
NXP Employee

Use the Debugger Shell to access memory. It is easier to use and supported.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,609 次查看
hwrobel
NXP Employee
NXP Employee

Use the Debugger Shell to access memory. It is easier to use and supported.

0 项奖励
回复
1,608 次查看
sinanakman
Senior Contributor III

Hi Heinz, how do you run the debugger shell ? is this part of CCS ?

This is the CCS I am running if the debugger shell is in another version  :

% show version

CCS Linux Release Build 365p0

CodeWarrior Connection Server version {4.13}

(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED

Thanks

Sinan Akman

0 项奖励
回复
1,608 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi,

You can open the debugger shell from CW: Window -> Show View -> Debugger Shell.

Marius

0 项奖励
回复
1,608 次查看
lunminliang
NXP Employee
NXP Employee

Hi, Kavita

Yes, as Heinz said. You can use "mem" or "display" in debugger shell, type "help mem" or "help display" for detail description of command.

0 项奖励
回复