Using sqrt() function in Codewarrior 6.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using sqrt() function in Codewarrior 6.2

跳至解决方案
4,754 次查看
jreyes085
Contributor I

Hello,

 

Im trying to use this function but it doesnt works...i put this in the header of the file that i want to use the function:

 

#include "math.h"       /* include math functions */

 

What i want to do is this....

 

irms=sqrt(sum2corriente/NUM_MCICLO);

 

//they are defined like (copy&paste from my main.c):

//#define NUM_MCICLO  100

//

//#pragma DATA_SEG DEFAULT

//static  dword sum2corriente=0;

//static  dword irms=0;

 

How could i do this? i know that sqrt(double variable), is this going to work? i want it to tried but i compile the file and it gives no errro, but when i pressed the debug button then it shows this error:

 

Error #1> Link error: Undefined: "sqrt"
              Referenced from "TPM1_ISR" in main.c
Error #2> Link Failed.

 

Im using the irms calc in a Interruption subroutine....

 

Please help! how can i get this to work?

 

Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,759 次查看
stanish
NXP Employee
NXP Employee

Seems the floating point library (e.g. ansif.lib) is not included in your project. I'd suggest you to see this thread

 

Attached is the list of libraries available in CodeWarrior for MCUs v6.2.

 

Stanish

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,760 次查看
stanish
NXP Employee
NXP Employee

Seems the floating point library (e.g. ansif.lib) is not included in your project. I'd suggest you to see this thread

 

Attached is the list of libraries available in CodeWarrior for MCUs v6.2.

 

Stanish

0 项奖励
回复
2,759 次查看
jreyes085
Contributor I

Thanks man! Gracias!

 

it works, i only create a new project and activate the floating point support...and it works!

 

Thanks, i was thinking of implement an asm algorithm to do the sqrt() function...

 

Thanks again!

0 项奖励
回复