Use qspi RAM for debugging MCF52223 with CodeWarrior 7.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use qspi RAM for debugging MCF52223 with CodeWarrior 7.1?

Jump to solution
2,297 Views
skyguy
Contributor III
Can QSPI RAM be used for debugging with CodeWarrior?  My application program won't exceed the flash size of an MCF52223, but it will exceed the SRAM size.  That will restrict my ability to debug.  I can add a QSPI RAM part to my development board to expand RAM, but before I do that, I want to make sure it has a chance of working.  I'm sure I saw this idea suggested, but I can't find it.
Thanks,
Rick
Labels (1)
0 Kudos
Reply
1 Solution
1,416 Views
skyguy
Contributor III
Won't work - here's the reply I got to a support request:
"SPI SRAM is not in MCF52233 memory range, so it is impossible to debug the code with CodeWarrior software.  You can consider to use MCF52259 MCU, which with 512KB internal Flash, 64KB internal RAM, and it also has Mini-Flexbus can connect with Max.  memory size 1MB SRAM memory chip."
Message Edited by skyguy on 2009-07-28 09:46 PM

View solution in original post

0 Kudos
Reply
1 Reply
1,417 Views
skyguy
Contributor III
Won't work - here's the reply I got to a support request:
"SPI SRAM is not in MCF52233 memory range, so it is impossible to debug the code with CodeWarrior software.  You can consider to use MCF52259 MCU, which with 512KB internal Flash, 64KB internal RAM, and it also has Mini-Flexbus can connect with Max.  memory size 1MB SRAM memory chip."
Message Edited by skyguy on 2009-07-28 09:46 PM
0 Kudos
Reply