Unable to program Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to program Flash

1,534件の閲覧回数
skurudi
Contributor II

Hi,

   I am using EN29LV320BT flash type, as it is not listed in Code Warrior 10.02 I have slected EN29LV640 flash type. I am  able to erase the flash. But when I try to program I get the following error

 

Downloading 0x00003200 bytes to be programmed at 0xFF840000  
CCSProtocolPlugin : Error writing registers [CCS last error: MBIST: core is RUNNING!]
Error:  Program operation failed.  Couldn't initialize registers

 

Could any body help?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,209件の閲覧回数
FridgeFreezer
Senior Contributor I

Taking a flying guess, the x320 part has half the space as the x640 part, so you're trying to program off the end of the device and getting an error.

 

You may be able to create a "correct" setting for the device by duplicating the x640 config and changing the relevant values.

0 件の賞賛
返信