Uboot flash problem on uncustom P2020RDB-PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot flash problem on uncustom P2020RDB-PC

Jump to solution
2,672 Views
huyang
Contributor III

Hi,

 

We got a problem on U-boot flash.

We changed the NOR Flash on P2020RDB-PC from 16MB(S29GL128P) to 64MB(S29GL512P).

And we got problem on uboot flash.

I know how to flash uboot using Codewarrior on custom board with 16MB NOR Flash.

What should we modify in process of uboot flash to 16MB NOR that we can flash uboot to 64MB NOR?

Thanks.

 

Best Regards,

Hu

Labels (1)
0 Kudos
Reply
1 Solution
2,360 Views
addiyi
NXP Employee
NXP Employee

Yes, you should modify the TLB and LAW to configure your new NOR mapping.

Adrian

View solution in original post

0 Kudos
Reply
3 Replies
2,360 Views
addiyi
NXP Employee
NXP Employee

You can map any peripheral (DDR, NOR, NAND, PCI and so on) to any addresses using a different memory range in TLB, LAW and CS (chip select). So, in your case you should modified the initialization file, to address your changes. Also, to program uboot in new NOR, in CodeWarrior Flash Programmer you should add S29GL512P into Flash Devices view.


Adrian

2,360 Views
huyang
Contributor III

So I should modify some value in p2020rdb-pc_init_core.tcl  which in P2020rdb project at Codewarrior?

Hu

0 Kudos
Reply
2,361 Views
addiyi
NXP Employee
NXP Employee

Yes, you should modify the TLB and LAW to configure your new NOR mapping.

Adrian

0 Kudos
Reply