UBoot flash problem with P2020RDB-PCA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UBoot flash problem with P2020RDB-PCA

ソリューションへジャンプ
2,132件の閲覧回数
huyang
Contributor III

Hi,

I got a problem when flash uboot.bin to our P2020RDB-PCA board by CW10.3.3.

I've done this whole procedure sucuessfully in July, but somehow it doesn't work now.

Here is console message, seems something wrong with verify step, is there anyone have similar problem?

 

8333_8333.jpgproblem.jpg

Is the address we set are wrong or there are other mistakes?

Please help us, Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,919件の閲覧回数
huyang
Contributor III

Hi,

Thanks for your specific interpretation.

We finnally found the problem that is our device selection setting is wrong.

We chose the device S29GL128P and the organization of it is 16Mx8x1, and that's the problem.

After we change the setting of the organization to 8Mx16x1, the problem solved.

Thanks again.

Hu

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,919件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi,

To program u-boot on P2020RDB-PCA board, I have followed the steps below:

- Enter in debug mode, using init file: P2020RDB-PC_init_core.tcl and mem file: P2020RDB-PC.mem;

- In Target Tasks, import: P2020DS_NOR_FLASH.xml

- In Add Program / Verifiy Action: check Erase sectors before program + Verify after program + Apply Address Offset (with address: 0xFFF80000)

- Switches on the board: SW2: OFF ON ON ON ON ON OFF ON and SW3: ON ON OFF OFF ON OFF ON OFF

Using setup above, I was able to program u-boot with no error.

Adrian

1,920件の閲覧回数
huyang
Contributor III

Hi,

Thanks for your specific interpretation.

We finnally found the problem that is our device selection setting is wrong.

We chose the device S29GL128P and the organization of it is 16Mx8x1, and that's the problem.

After we change the setting of the organization to 8Mx16x1, the problem solved.

Thanks again.

Hu

0 件の賞賛
返信