The address problem about p2020rdb in Codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The address problem about p2020rdb in Codewarrior

Jump to solution
2,163 Views
敏赵
Contributor I

Hello there,

I an designing a product using p2020cpu refering to the design of p2020rdb-pc. I have 4GB DDR, 32MB Nor Flash. My memory map:

                               0x0_0000_0000  0x0_ffff_ffff   DDR

                               0x1_e000_0000  0x1_e00f_ffff  CCSRBAR                                          

                               0xf_fe00_0000   0xf_ffff_ffff     NOR  (0xf_eff8_0000 uboot)

I have modify the base address of nor in LAW to 0xFFE000000,and the NOR configuration in MMU.

Now I found the following codes in p2020rdb_pc_init_rom.tcl.

# L2SRBAR0

# bit 0-17 = BASE addr: 0xFFFC0000

mem [CCSR 0x20100] = 0xFFFC0000

1)Why the L2SRBAR0 base address at 0xfffc0000 in p2020rdb-pc? Should I modify the address in my board?

 

# Set interrupt vectors in SRAM

# IVPR

reg ${SPR_GROUP}IVPR = 0xFFFF0000

# debug - (a valid instruction should exist to be fetched)

reg ${SPR_GROUP}IVOR15 = 0x0000F000

# program

reg ${SPR_GROUP}IVOR6 = 0x0000F700

 

# Put a valid opcode at debug and program exception vector addresses

mem v:0xFFFFF000 = 0x48000000

mem v:0xFFFFF700 = 0x48000000

 

Need I modify the code above?

 

Best regards,

Min Zhao

Labels (1)
0 Kudos
Reply
1 Solution
1,944 Views
yipingwang
NXP TechSupport
NXP TechSupport

# bit 0-17 = BASE addr: 0xFFFC0000

mem [CCSR 0x20100] = 0xFFFC0000

# L2SRBAREA0

# bit 28-31 = EXTENTED BASE addr: 0x0000000f

mem [CCSR 0x20104] = 0x0000000f


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,944 Views
yipingwang
NXP TechSupport
NXP TechSupport

This initialization file is used in ROM version project debugging(for example debug program running on NOR Flash).

After reset, e500 cores need to run before being able to enter debug mode.

Work-around: set a HW BP at reset address and run the core; after the core hits the BP, it enters debug mode

e500 cores need to have valid opcode at the interrupt vector, so temporarily use SRAM for this purpose.

In this initialization file, internal SRAM is configured at highest memory address to cover the default 4k MMU page.

# L2CTL

# bit 0 = 0        - L2E: L2 SRAM disabled

# bit 1 = 0            - L2I: L2 invalidate

# bit 2-3 = 10        - L2SIZ: = 512K

# bit 13-15 = 010    - L2SRAM: One half is SRAM (256K)

mem [CCSR 0x20000] = 0x60020000

# L2SRBAR0

# bit 0-17 = BASE addr: 0xFFFC0000

mem [CCSR 0x20100] = 0xFFFC0000

# L2SRBAREA0

# bit 28-31 = EXTENTED BASE addr: 0x00000000

mem [CCSR 0x20104] = 0x00000000

Please refer to the following register definition.

pastedImage_0.png

No need to change these debug related configurations, actually I don't think this initialization file is suitable for your current task(board bringing up).


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,944 Views
敏赵
Contributor I

I can't find where should I modify in the rom.tcl file.

Best regards,

Min Zhao

0 Kudos
Reply
1,944 Views
yipingwang
NXP TechSupport
NXP TechSupport

# L2SRBAREA0

# bit 28-31 = EXTENTED BASE addr: 0x00000000

mem [CCSR 0x20104] = 0x00000000

1,944 Views
敏赵
Contributor I

Do you mean my base address is not 0x00000000? What's my 22-bit L2 memory-mapped SRAM base address?

Best regards,

Min Zhao

0 Kudos
Reply
1,945 Views
yipingwang
NXP TechSupport
NXP TechSupport

# bit 0-17 = BASE addr: 0xFFFC0000

mem [CCSR 0x20100] = 0xFFFC0000

# L2SRBAREA0

# bit 28-31 = EXTENTED BASE addr: 0x0000000f

mem [CCSR 0x20104] = 0x0000000f


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply