TWR-LS1021A Flash Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-LS1021A Flash Programming

1,786件の閲覧回数
christopherbisc
Contributor II

I am working with an LS1021A CPU on a customized board based on the TWR-LS1021A reference board.

For programming the Flash I am using Codewarrior USB Tap and CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA IDE.

Is there any possibility to program the Flash without the CodeWarrior Development Studio and the corresponding license for the production flow. Like a Standalone programmer, or a free version of Codewarrior?

0 件の賞賛
返信
1 返信

1,564件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Christopher Bischof,

There is a 30 days free evaluation license for the customer to use CodeWarrior.

For LS1021A custom board bringing up and flash programming, the customer needs to purchase the Developer Level Suite.

Except using CodeWarrior, you also could consider to set up SD/MMC u-boot, then program flash under SD u-boot.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信