T1024 XFI serdes validation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1024 XFI serdes validation

1,326件の閲覧回数
sureshk
Contributor II

Hi,

  In our custom board using T1024 we are using XFP module. we performed the serdes validation using QCVS tool , BIST test is passing for digital loop back. and external loop back test also passing for test pattern  HFTP and PRBS7 test patterns.

      But while testing with data pattern HHFTP , in external loopback , with bits upto 4.10E+04 this test is passing. For above these bits CDR lock and BIST pattern sync are passing but showing some error count. what causes for this error count ?

 

 

Kindly suggest the test patterns to be used for evaluating the XFP interface.

 

156542_156542.pngpastedImage_0.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)