Software Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software Interrupt

4,314 Views
Jules
Contributor I
Hello,

is there a possibility to cause an interrupt via Software(maybe with an assembler instruction or something else)??
I am using the MPC565.

Thanks,

Julian
Labels (1)
0 Kudos
Reply
2 Replies

2,283 Views
Teo
NXP Employee
NXP Employee
You could use:
- System call ("sc" mnemonic). Usually used for calls into OS kernels
- Unconditional trap instructions. Usually used for software breakpoints
- Program interrupt. i.e. an illegal opcode. Usually this is used as an alternative to unconditional trap for software breakpoints
- Debug interrupt. i.e. putting a hardware breakpoint when a PC has a sertain address.

Note that with exception of the first solution, you might interfier with the debugger. i.e. debugger to think the processors stopped due to its breakpoints, and your interrupt handler routine will never be called when you a debugging the application.

Best regards,
Teo
0 Kudos
Reply

2,283 Views
Jules
Contributor I
Thank you Teo,

but i don't know if this is the right for me.
Could i assing several priority levels wit the "system call"?

I am programming a simple preemptive OS(3 tasks).
For this i need two several priority levels for my tasks one higher then the other.
The PIT should cause the change by causing one of the two interrupts.

Best wishes,

Julian
0 Kudos
Reply