So many methods of installing QCVS failing!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

So many methods of installing QCVS failing!

1,008 次查看
Greg5_as_suggested
Contributor I

Hi all,

 

We are trying to install QCVS in order to generate correct DDR3 settings on a PowerPC QORIQ SoC T1040.

 

We are trying to use this tool: CodeWarrior® Dev Tools for Networked Apps | NXP Semiconductors but we need to add in QCVS

 

I am trying to evaluate the product under the short trial period, but so far it doesn't even have the basic PowerPC DDR3 tools to do anything useful.

 

The link here: Solved: Re: where can i download QCVS4.5 offline installation package for CW10.5.1 for power pc - NX... points me to a google drive, but I can't find any file there - please help.

 

 

On CodeWarrior for Power Architecture [Version: 10.5.1 , Build Id:160128] I went to "Help/Install new software" and set the "Work With" drop down to point to QCVS, but get error messages just saying "Unable to read the repository... org.eclipse.equinox.p2.core.ProvisionException".

I've tried the following repos:

--- FSL PA Build Tools - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.buildtools_win

--- FSL PA Packet Tools - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.pkt_win

--- FSL PA QCVS - http://cache.nxp.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win

--- FSL PA QCVS - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win

 

Thanks, 
~Greg

标记 (2)
0 项奖励
回复
2 回复数

984 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please download "QCVS offline installation packages for CodeWarrior for Power Architectures Rev 4.5" from https://support.nxp.com/s/case/5002p00002zpIBRAA2/community-so-many-methods-of-installing-qcvs-faili...

After downloading QCVS for PA 4.5, please open CodeWarrior for PA 10.5.1 IDE, then install QCVS package from "Help->Install New Software->Add->Archive".

0 项奖励
回复

727 次查看
petes1
Contributor II
This link is no longer working?
0 项奖励
回复