Simulate in CW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,731件の閲覧回数
Futte
Contributor II

I want the simulate a MCF52254 in CW V10.2, and i have trouble finding the settings where i can choose "Full chip simulate".

 

I hope you guys can help me...

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,568件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Full Chip Simulation (FCS) is only available for the S08 cores.

 

BK

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,569件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

Full Chip Simulation (FCS) is only available for the S08 cores.

 

BK

0 件の賞賛
返信