Serious Bug in Codewarrior 7.2 coldfire MCF52277

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serious Bug in Codewarrior 7.2 coldfire MCF52277

1,478 Views
tonytrm
Contributor II

Please see the S Record below. The first line is correct but then at the same address is 4E4E5600004BFAFFFE41FA0004D1, This over writes the real code, so there is no way this code can be used to make romable code. Can anyone help? I have never seen this sort of problem before.

 

 

S311000000004D454D53000001700001000A40
S321000000004E5600004BFAFFFE41FA0004D1FC0000083E700143FA0004D3FC000025
S3210000001C0A324E914E5E4E754E560000223C0000016E7000207C00000000D1CD1D
S3210000003843FA0004D3FC00000A3A4E91700441FA0004D1FC000001AC4E9041FA2D
S321000000540004D1FC00000748700143FA0004D3FC000009F44E914E5E4E7551FC51
S321000000704E560000207C00000000D1CD7203B081630270007400143008157201CD
S3210000008CB48167067202B081650E41FA0004D1FC000000A44E90600C41FA00045F
S321000000A8D1FC000000564E904E5E4E754E5600002F07207C00000000D1CD74033B
S321000000C4B082630470FF602E7E001E3008157401BE8267067402B082650E41FA23
S321000000E00004D1FC000000804E90600C41FA0004D1FC0000002E4E9070002E1F8E

Labels (1)
0 Kudos
Reply
1 Reply

936 Views
CrasyCat
Specialist III

Hello

 

I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

CrasyCat

0 Kudos
Reply