Scan timeout during secure debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Scan timeout during secure debug

2,257 次查看
SergioS
Contributor II

Dear all

I've configured a LS1012A board to manage secure debug (level 2)

When I try to connect to target CCS and CodeWarrior studio return the error "Scan timeout"

I've seen that this bug is documented in the release notes of 11.2 version (DTCCS-124

Issue: [LS1043][SecureDebug] CCS returns Scan timeout when trying to
config chain

Workaround: none

Now I'm using v11.5.5 but the problem is the same. Does anybody know the status of this bug?

Thanks and regards

Sergio

0 项奖励
回复
1 回复

2,225 次查看
yipingwang
NXP TechSupport
NXP TechSupport
0 项奖励
回复