Saving Flash Programmer erase range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Saving Flash Programmer erase range

2,955件の閲覧回数
Richly
Contributor III
Every time I reload the IDE, I also have to load the settings for the processor I'm using.  Then, I have to open the Erase/Blank Check page of the Flash Programmer and select the range to erase (0x0 to 0x1FFFF, the maximum that can be programmed with the SE version of the CodeWarrior IDE).   My attempts to save the configuration file with the erase range set have not been successful.

So, my questions are
1) is there a way to specify the range to be erased in the Flash Programmer's configuration (.xml) file that I have to load?
2) is there a manual for the Flash Programmer that explains what all the entries in this file are?
3) what progress has been made on the request (now about two years old) that debugging Flash programs be about as easy as debugging RAM programs?

Thanks
    - R
ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,610件の閲覧回数
J2MEJediMaster
Specialist I
Now would be a good time to remind folks posting to the forums that you need to identify (preferably in the posting's subject line) the processor and CodeWarrior version you're using, please. I could guess that maybe you're talking about ColdFire...

---Tom
0 件の賞賛
返信

1,610件の閲覧回数
Richly
Contributor III
Sorry.  My questions are about CodeWarrior Development Studio for ColdFire Architectures Version 7.0, Build 15.  In case it makes a difference, the processor is the MCF52233.
    - R
0 件の賞賛
返信

1,610件の閲覧回数
CrasyCat
Specialist III
Hello
 
It does not look like this is supported.
 
If you feel like this is a feature you would need to have in future release of the tool, I would recommend you to submit a Service Request .
 
I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to Specify Technical request as category, CodeWarrior as Topic
Specify you are requesting a change/extension in the Flash programmer tool.
 
CrasyCat
0 件の賞賛
返信