Sample Source code for MPC7410

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample Source code for MPC7410

3,545 Views
Muneer
Contributor II
hi

I'm using CW8.7 and my target is MPC7410
Any sample source code avaible as a project...
i tried in CW8.7 samples, in that i'm not getting any idea...

plz suggest me, where i can get sample...

Muneer
Labels (1)
0 Kudos
Reply
3 Replies

1,923 Views
J2MEJediMaster
Specialist I
It's not clear to me why you need a sample project targeting a specific processor. What CPU feature are you trying to make use of?

---Tom

0 Kudos
Reply

1,923 Views
Muneer
Contributor II
Hi

I'm new to this processor...
Actually i need boot code, basic register settings in MPC7410.
To MPC7410 processor Flash is interfaced for this how to do settings & what are all registers to be init

Muneer
0 Kudos
Reply

1,923 Views
Black
Contributor I
I recommend creating a stationery project with CodeWarrior EPPC New Project Wizard and Freescale PowerPC EABI Linker for MPC7410 and your evaluation board then add your own code to this project that can be used as a starting point. The stationery project has the minimal setup and code to get your evaluation board up and running. For more details please consult the stationery project readme files.
 
Please note that the current version of CodeWarrior for Power Architecture is 8.8.1 and it is available for download as an evaluation version here.
0 Kudos
Reply