SPI Multi Slave Communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Multi Slave Communication

1,501件の閲覧回数
joginderrana
Contributor II

HI, I am very new to Freescale Kinetic microcontrollers. I am working on FRDM-k20d50m development board and trying to develop an application to interface two slaves on this development board. My requirement is to send data to 1st slave and then receive data from the same slave and then to deploy same operation on 2nd slave. If I am using one slave at a time and disconnect the other one then it works fine but if I connect two slaves the at same time I am not receiving any data from slave. The basic code to initiate SPI communication between two slaves is as below:

 

/* Below block of code writes/reads data from first slave*/

 

  SM1_SelectConfiguration(SPI, ChipSelect, AttributeSet);

  SM1_SendBlock(SPI, out_data, sizeof (out_data));

  SM1_ReceiveBlock(SPI, &in_data, sizeof (in_data));

 

  /* Below block of code writes/reads data from second slave*/

 

  SM1_SelectConfiguration(SPI, ChipSelect_1, AttributeSet_1);

    SM1_SendBlock(SPI, out_data, sizeof (out_data));

        SM1_ReceiveBlock(SPI, &in_data_1, sizeof (in_data_1));

 

Please help me to make the communication possible with two slaves at the same time with proper toggling.

ラベル(1)
0 件の賞賛
返信
1 返信

1,139件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

To investigate your problem correctly and efficiently, please provide us the follows: 1. your CW version: Start the IDE and click on Help | About CodeWarrior Development Studio. Send me the version and build id. 2. send the entire sample code folder(include .project, prm,c...) in zip format to me. so that i can test it on my side directly. 3.      error screenshot. thanks!

0 件の賞賛
返信