Running External Tool after Build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running External Tool after Build

1,974 Views
Craigt
Contributor I
We are using the CodeWarrior for the PowerPC (MobileGT Processor Edition) and have the following question related to the build process that I hope some one can help with.  After the build is complete we would like to run an external tool to add a digital signature to the created ROM image.  I do not see a place in the environment where you can automatically have the environment  execute an external tool after the build/make is complete.  Does anyone know if the tool would support this feature?


Thanks,

Craig
Labels (1)
0 Kudos
Reply
1 Reply

1,014 Views
BlackNight
NXP Employee
NXP Employee
Hi Craig,
I do not have the MobileGT version, but if you go to the project settings/preference panel, under Target > Target Settings, there is an option where you can set up a Post-Linker: BatchRunner Postlinker. This will provide you another panel (Linker > BatchRunner PostLinker) where you shall be able to specify what you need.

Erich
0 Kudos
Reply