Reading DIMM SPD using CW 11.2.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading DIMM SPD using CW 11.2.3

2,826件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Community,

I am trying getting the SPD information from DIMM with QCVS tool.

I have followed procedure as section "1.2.3.1 Using Read from SPD option" in QCVS DDR Tool User Guide. (Rev, 4.x, 09/2017) But, I got the below error log after click "Read SPD" button. What should I check to solve this error?

[Environment]

  Board : LS1046A RDB * DIP switches and Jumpers are set to default.

  SW : CODEWARRIOR Version 11.2.3 / Build Id : 170322

[Error]

pastedImage_2.png

Best Regards,

Kazuma Sasaki.

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,591件の閲覧回数
addiyi
NXP Employee
NXP Employee

The version is the correct one. Indeed it looks like the problem was generated during update, maybe because of a network issue.

Adrian

0 件の賞賛
返信

2,591件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please provide information about QCVS version. Click on the highlighted icon and provide info.

pastedImage_1.png 

Adrian

0 件の賞賛
返信

2,591件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Adrian,

My QCVS version is 4.10.0.0001-20170917.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信

2,592件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Community,

I solved this issue by my self.

When I get above error, I only see "flash" and "SA" folder at <CW4NET_version>\CW_ARMv8\Config.

I copied other configuration data(SoCs, and boards folder) from other PC. then, I can read SPD information from DIMM correctly.

So, I suppose my installation process anythings wrong. I should re-install CodeWarrior to solve this issue. thanks.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信