QorIQ hardware device tree editor is missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QorIQ hardware device tree editor is missing

跳至解决方案
3,676 次查看
rahulr
Contributor II

I created a new QorIQ configuration project in CodeWarrior. The hardware device tree editor is missing from the configuration tools option. I am using LS1021A processor, is the device tree editor not available for LS1021?

 

173436_173436.pngScreenshot from 2016-12-23 22-10-43.png

 

Here's my system config

Ubuntu 16.04

CodeWarrior - 10.0.8

QorIQ configuration and validation tool - 4.6

 

ls1021a qoriq devicetree

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
3,163 次查看
addiyi
NXP Employee
NXP Employee

Device tree for the new SoCes is not available.

Adrian

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,164 次查看
addiyi
NXP Employee
NXP Employee

Device tree for the new SoCes is not available.

Adrian

0 项奖励
回复
3,163 次查看
ACGarland
Contributor III

It is now nearly a year later. Is this still the case?

I'm working with the LS1012A using CW 11.2.5. I'm not seeing any support within CW for device tree editing either.

0 项奖励
回复
3,163 次查看
ACGarland
Contributor III

Since my previous post, I found documentation on the DT editor, part of the Processor Expert, within the CW install directory:

/usr/local/Freescale/CW4NET_v2017.03/Common/QCVS/ProcessorExpert/Help/PDF/Hardware Device Tree Configuration - User Guide.pdf

Haven't tried to us it yet, but at least it appears to be available.

0 项奖励
回复
3,163 次查看
ACGarland
Contributor III

Well, it appears I spoke too soon--the documentation mentions the device tree configuration, but the QCVS module listing for the LS1012A doesn't include such a module.

Screen Shot 2017-11-17 at 3.21.09 PM.png

What is the recommended approach to developing device tree information for the LS1012A in the absence of this module within QCVS?

0 项奖励
回复