RUN/PAUSE LED RED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RUN/PAUSE LED RED

2,045 Views
Ellu24
Contributor III

I am trying to connect lS1046RDB through CWTAP. Then TX/RX led is green and RUN/PAUSE led is red. How can I resolve this problem?

Thanks in advance

0 Kudos
Reply
1 Reply

2,023 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please download CW4NET_v2020.06 from the following link and install it on your PC.
https://drive.google.com/file/d/1Kjq1nLYrtIfWAHYrup5Cf-TTEJI9iWiu/view?usp=sharing

Please download armv8 11.5.5 pack form the following link and open CodeWarrior IDE to install it from Help->Install New Software->Add->Archive.
https://drive.google.com/file/d/1ZHiYWDOhb27o0oD5Brqjn4_vJzRUCKoY/view?usp=sharing

Please don't plug in CodeWarrior TAP when installing CodeWarrior software.

Please open C:\Freescale\CW4NET_v2020.06\Common\CCS\bin\ccs.exe and type the following commands and let me know the result.

(bin) 1 % delete all
(bin) 2 % config cc cwtap
(bin) 3 % show cc

 

0 Kudos
Reply