RCW in T2080

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RCW in T2080

2,120件の閲覧回数
monalihaware
Contributor III

1. If RCW value is over written by the CFG file, does the "Reset Control Word Status Register n"  get updated? or

it shows the values fetched with Hard coded RCW ?

タグ(2)
0 件の賞賛
返信
1 返信

1,894件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Monali Haware,

The RCW value provided in CodeWarrior JTAG configuration file will override RCW configuration on the target board.

Please refer to the section "8.2 Using a JTAG configuration file to override RCW" in C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信