RCW in T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RCW in T2080

2,123 Views
monalihaware
Contributor III

1. If RCW value is over written by the CFG file, does the "Reset Control Word Status Register n"  get updated? or

it shows the values fetched with Hard coded RCW ?

Tags (2)
0 Kudos
Reply
1 Reply

1,897 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Monali Haware,

The RCW value provided in CodeWarrior JTAG configuration file will override RCW configuration on the target board.

Please refer to the section "8.2 Using a JTAG configuration file to override RCW" in C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply