Query:  level of usage for USB Tap + Cross-triggering feature + P5040/21

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query:  level of usage for USB Tap + Cross-triggering feature + P5040/21

Jump to solution
1,302 Views
robertsierra
NXP Employee
NXP Employee

What is the probability of is using a USB Tap && utilizing Cross-triggering && using a  P5040/21 via CW for Power Architectures (non-automotive/MCU  version)?   Need a rough order magnitude type of indicator…  (Never, often, everyday)

 

Labels (1)
0 Kudos
Reply
1 Solution
1,154 Views
marius_grigoras
NXP Employee
NXP Employee

Hi Robert,

As far I know, I don't think this scenario is very used. Btw, the cross triggering works for P5040/21DS, but for P5040/21RDB (that will be provided in the next PA SP) is not working (due of CR:ENGR00268643 that cannot be integrated via SP).

Regards,

Marius

View solution in original post

0 Kudos
Reply
2 Replies
1,155 Views
marius_grigoras
NXP Employee
NXP Employee

Hi Robert,

As far I know, I don't think this scenario is very used. Btw, the cross triggering works for P5040/21DS, but for P5040/21RDB (that will be provided in the next PA SP) is not working (due of CR:ENGR00268643 that cannot be integrated via SP).

Regards,

Marius

0 Kudos
Reply
1,154 Views
lunminliang
NXP Employee
NXP Employee

Not quite understand the question?

0 Kudos
Reply