Query:  level of usage for USB Tap + Cross-triggering feature + P5040/21

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Query:  level of usage for USB Tap + Cross-triggering feature + P5040/21

跳至解决方案
1,294 次查看
robertsierra
NXP Employee
NXP Employee

What is the probability of is using a USB Tap && utilizing Cross-triggering && using a  P5040/21 via CW for Power Architectures (non-automotive/MCU  version)?   Need a rough order magnitude type of indicator…  (Never, often, everyday)

 

标签 (1)
0 项奖励
回复
1 解答
1,146 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi Robert,

As far I know, I don't think this scenario is very used. Btw, the cross triggering works for P5040/21DS, but for P5040/21RDB (that will be provided in the next PA SP) is not working (due of CR:ENGR00268643 that cannot be integrated via SP).

Regards,

Marius

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,147 次查看
marius_grigoras
NXP Employee
NXP Employee

Hi Robert,

As far I know, I don't think this scenario is very used. Btw, the cross triggering works for P5040/21DS, but for P5040/21RDB (that will be provided in the next PA SP) is not working (due of CR:ENGR00268643 that cannot be integrated via SP).

Regards,

Marius

0 项奖励
回复
1,146 次查看
lunminliang
NXP Employee
NXP Employee

Not quite understand the question?

0 项奖励
回复