Query:  level of usage for USB Tap + Cross-triggering feature + P5040/21

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query:  level of usage for USB Tap + Cross-triggering feature + P5040/21

ソリューションへジャンプ
1,313件の閲覧回数
robertsierra
NXP Employee
NXP Employee

What is the probability of is using a USB Tap && utilizing Cross-triggering && using a  P5040/21 via CW for Power Architectures (non-automotive/MCU  version)?   Need a rough order magnitude type of indicator…  (Never, often, everyday)

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,165件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi Robert,

As far I know, I don't think this scenario is very used. Btw, the cross triggering works for P5040/21DS, but for P5040/21RDB (that will be provided in the next PA SP) is not working (due of CR:ENGR00268643 that cannot be integrated via SP).

Regards,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,166件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi Robert,

As far I know, I don't think this scenario is very used. Btw, the cross triggering works for P5040/21DS, but for P5040/21RDB (that will be provided in the next PA SP) is not working (due of CR:ENGR00268643 that cannot be integrated via SP).

Regards,

Marius

0 件の賞賛
返信
1,165件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Not quite understand the question?

0 件の賞賛
返信