QorlQ Configuration error: Target processor not selected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorlQ Configuration error: Target processor not selected

ソリューションへジャンプ
3,382件の閲覧回数
nsutch
Contributor III

Hi,

I'm trying to setup a new QorIQ Configuration Project for a T1040 processor. I've selected the processor and die revision in the wizard setup but once I complete the wizard I get 'Error: Target procssor is not selected'. I've tried navigating through the 'Components Library Tab' to 'Processors' and reselcting the processor but it makes no differnce.

CodeWarrior details:

CodeWarrior Development studio for Power Architecture v10.5.0

QorIQ Configuration and Validation Suite v4.4.1

License type - Evaluation

Any help to clear this error would be appreciated.

Thanks,

Nick

ラベル(1)
0 件の賞賛
返信
1 解決策
3,025件の閲覧回数
addiyi
NXP Employee
NXP Employee

It is better to update CW to 10.5.1. This way the update site containing qcvs 4.5 will be visible. If not, please use http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win not http://freescale.com/lgfiles/updates/Eclipse/PA10_5_0/com.freescale.pa.qcvs_win

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,025件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please update to QCVS 4.5. To do that go to Help > Install New Software and select FSL PA QCVS - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win as update site.

Make sure not ccs/cdde/python processes are running during installation.

Adrian

0 件の賞賛
返信
3,025件の閲覧回数
nsutch
Contributor III

Adrian,

Thaks for the quick response. I followed the steps you mentioned but I can still only see version 4.4.1. See image below:

Available Software.jpg

Is there a way to manually update to 4.5?

Thanks,

Nick

0 件の賞賛
返信
3,025件の閲覧回数
nsutch
Contributor III

Thanks Adrian, that worked.

0 件の賞賛
返信
3,026件の閲覧回数
addiyi
NXP Employee
NXP Employee

It is better to update CW to 10.5.1. This way the update site containing qcvs 4.5 will be visible. If not, please use http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win not http://freescale.com/lgfiles/updates/Eclipse/PA10_5_0/com.freescale.pa.qcvs_win

Adrian

0 件の賞賛
返信