QorIQ hardware device tree editor is missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ hardware device tree editor is missing

ソリューションへジャンプ
3,695件の閲覧回数
rahulr
Contributor II

I created a new QorIQ configuration project in CodeWarrior. The hardware device tree editor is missing from the configuration tools option. I am using LS1021A processor, is the device tree editor not available for LS1021?

 

173436_173436.pngScreenshot from 2016-12-23 22-10-43.png

 

Here's my system config

Ubuntu 16.04

CodeWarrior - 10.0.8

QorIQ configuration and validation tool - 4.6

 

ls1021a qoriq devicetree

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
3,182件の閲覧回数
addiyi
NXP Employee
NXP Employee

Device tree for the new SoCes is not available.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,183件の閲覧回数
addiyi
NXP Employee
NXP Employee

Device tree for the new SoCes is not available.

Adrian

0 件の賞賛
返信
3,182件の閲覧回数
ACGarland
Contributor III

It is now nearly a year later. Is this still the case?

I'm working with the LS1012A using CW 11.2.5. I'm not seeing any support within CW for device tree editing either.

0 件の賞賛
返信
3,182件の閲覧回数
ACGarland
Contributor III

Since my previous post, I found documentation on the DT editor, part of the Processor Expert, within the CW install directory:

/usr/local/Freescale/CW4NET_v2017.03/Common/QCVS/ProcessorExpert/Help/PDF/Hardware Device Tree Configuration - User Guide.pdf

Haven't tried to us it yet, but at least it appears to be available.

0 件の賞賛
返信
3,182件の閲覧回数
ACGarland
Contributor III

Well, it appears I spoke too soon--the documentation mentions the device tree configuration, but the QCVS module listing for the LS1012A doesn't include such a module.

Screen Shot 2017-11-17 at 3.21.09 PM.png

What is the recommended approach to developing device tree information for the LS1012A in the absence of this module within QCVS?

0 件の賞賛
返信