QCVS device tree editor not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS device tree editor not working

2,285 Views
PaulWalker
Contributor IV

I using Code Warrior for PA 10.5.1 and QCVS 4.5.

I'm trying to use the Hardware Device Tree feature but it is giving me trouble.

The online help says the GUI editor offers Insert/Remove options for adding, editing and removing nodes. I get no options for manipulating nodes.

If I create a project starting with an empty tree, I cannot add anything to it. The GUI editor does not allow editing, and a 'top' dts source file is not created.

If a import an existing dts, I can only change via the import file. The GUI editor does not allow editing.

Press F1 for help does not give any context help for a selected node.

This all suggests QCVS is might not be working correctly. I've tried numerous re-installs but no change.

Any idea?

Thanks

0 Kudos
Reply
3 Replies

2,276 Views
yipingwang
NXP TechSupport
NXP TechSupport

I have verified device tree editor in QCVS 4.5, GUI editor doesn't work normally, the same as your description.

0 Kudos
Reply

2,273 Views
PaulWalker
Contributor IV

Can anything be done? I'm using an offline install package for QCVS as online updating is not working.

0 Kudos
Reply

2,172 Views
yipingwang
NXP TechSupport
NXP TechSupport

QCVS 4.5 is the latest.

0 Kudos
Reply