QCVS Installation Directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS Installation Directory

Jump to solution
5,571 Views
richpohle
Contributor I

In section 3.2 "Installation over Eclipse" of the QCVS Installation Guide, h t t p://freescale.com/lgfiles/updates/Eclipse/QCVS. However this website is no longer active since the Freescale website was converted to NXP. However, simply replacing the freescale with nxp in the above URL it does not work either. Both of these addresses are redirected to the main www.nxp.com website.

Note: for the above address, the http is intentionally entered here only with spaces so this interface does not convert it automatically to www.nxp.com.

Labels (1)
0 Kudos
Reply
1 Solution
2,707 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Rich,

Issue has been resolved please test the regular  http://freescale.com/lgfiles/updates/Eclipse/QCVS

Regards,

View solution in original post

0 Kudos
Reply
4 Replies
2,708 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Rich,

Issue has been resolved please test the regular  http://freescale.com/lgfiles/updates/Eclipse/QCVS

Regards,

0 Kudos
Reply
2,707 Views
addiyi
NXP Employee
NXP Employee

Please use http://nxp.com/lgfiles/updates/Eclipse/QCVS  as update site. The migration from freescale.com to nxp.com was completed.

Adrian

0 Kudos
Reply
2,707 Views
richpohle
Contributor I

Is this site down? I tried to perform an update and got an error message as a result.

Is there an alternate method to install the QCVS in Eclipse.

Screenshot from 2015-12-08 08_40_13.png

0 Kudos
Reply
2,707 Views
addiyi
NXP Employee
NXP Employee

Because of site migration sometime, when I tried to access updatesite I get

Connection timed out: connect

Unable to connect to repository

In short time, this kind of problem will be resolved.

Adrian

0 Kudos
Reply