QCVS Installation Directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS Installation Directory

ソリューションへジャンプ
5,499件の閲覧回数
richpohle
Contributor I

In section 3.2 "Installation over Eclipse" of the QCVS Installation Guide, h t t p://freescale.com/lgfiles/updates/Eclipse/QCVS. However this website is no longer active since the Freescale website was converted to NXP. However, simply replacing the freescale with nxp in the above URL it does not work either. Both of these addresses are redirected to the main www.nxp.com website.

Note: for the above address, the http is intentionally entered here only with spaces so this interface does not convert it automatically to www.nxp.com.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,635件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Rich,

Issue has been resolved please test the regular  http://freescale.com/lgfiles/updates/Eclipse/QCVS

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,636件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Rich,

Issue has been resolved please test the regular  http://freescale.com/lgfiles/updates/Eclipse/QCVS

Regards,

0 件の賞賛
返信
2,635件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please use http://nxp.com/lgfiles/updates/Eclipse/QCVS  as update site. The migration from freescale.com to nxp.com was completed.

Adrian

0 件の賞賛
返信
2,635件の閲覧回数
richpohle
Contributor I

Is this site down? I tried to perform an update and got an error message as a result.

Is there an alternate method to install the QCVS in Eclipse.

Screenshot from 2015-12-08 08_40_13.png

0 件の賞賛
返信
2,635件の閲覧回数
addiyi
NXP Employee
NXP Employee

Because of site migration sometime, when I tried to access updatesite I get

Connection timed out: connect

Unable to connect to repository

In short time, this kind of problem will be resolved.

Adrian

0 件の賞賛
返信