QCVS DDR Validation Connection Refused

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS DDR Validation Connection Refused

9,041 Views
rodneymclendon
Contributor I

I'm trying to run a validation on the DDR controllers, however the connection is always refused regardless of the JTAG clock speed chosen.  The CW is v10.5.1, and QCVS is v4.5.  The connection setup is as follows:

 

 

166971_166971.jpgMyPicture1.jpg

 

 

The log from the ccs server is:

 

(bin) 2 %
CCSAPI connection #1 accepted from vmware-localhost at Tue Nov 01 16:22:50 2016
check_min_version(serverh=0,*version)
  api version: 00000004 00000006
available_connections(serverh=0,*count,*cc)
  connections: {0,73,0x0a0f9209}
cc_version(serverh=0,cc_index=0,index=0,*version)
  ERROR(10): Connection refused
get_remote_user(serverh=0,cc_index=0,*remote_user_hostname,count)
  user:ASH-5WLWZ12.INT.CW.LOCAL
CCSAPI connection #1 from vmware-localhost closed at Tue Nov 01 16:22:55 2016
(bin) 2 %

 

Rodney

Labels (1)
0 Kudos
Reply
23 Replies

771 Views
rodneymclendon
Contributor I

It also appears the CCS does not find the CW tap (i.e., findcc cwtaps -eth does not return anything, even after running setup.exe).

0 Kudos
Reply

771 Views
addiyi
NXP Employee
NXP Employee

Try several times the ccs command findcc cwtaps -eth. There was an issue in ccs (I think in your ccs version it is present) where the ccs is not able to discover all the devices from network.

 

Are the cwtap and your pc in the same sub-network?

Adrian

0 Kudos
Reply

771 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rodney McLendon,

1. Please check whether CDDE path is valid in Hardware configuration manager window, for example <Installation path>\eclipse\Optimization\target-connection\cdde\cdde-windows\bin\cdde.exe.

2. In the CCS console, please enter the following commands and check the result.

(bin) 7 % config cc cwtap:10.15.146.9
(bin) 8 % show cc
CodeWarrior TAP Boot Loader version 1.0.1
CodeWarrior TAP OS version 1.0.1

3. Do you have a valid DDRv license deployed in <INSTALL_DIR>\eclipse\ProcessorExpert\?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply