QCVS DDR Validation Connection Refused

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS DDR Validation Connection Refused

9,034件の閲覧回数
rodneymclendon
Contributor I

I'm trying to run a validation on the DDR controllers, however the connection is always refused regardless of the JTAG clock speed chosen.  The CW is v10.5.1, and QCVS is v4.5.  The connection setup is as follows:

 

 

166971_166971.jpgMyPicture1.jpg

 

 

The log from the ccs server is:

 

(bin) 2 %
CCSAPI connection #1 accepted from vmware-localhost at Tue Nov 01 16:22:50 2016
check_min_version(serverh=0,*version)
  api version: 00000004 00000006
available_connections(serverh=0,*count,*cc)
  connections: {0,73,0x0a0f9209}
cc_version(serverh=0,cc_index=0,index=0,*version)
  ERROR(10): Connection refused
get_remote_user(serverh=0,cc_index=0,*remote_user_hostname,count)
  user:ASH-5WLWZ12.INT.CW.LOCAL
CCSAPI connection #1 from vmware-localhost closed at Tue Nov 01 16:22:55 2016
(bin) 2 %

 

Rodney

ラベル(1)
0 件の賞賛
返信
23 返答(返信)

769件の閲覧回数
rodneymclendon
Contributor I

It also appears the CCS does not find the CW tap (i.e., findcc cwtaps -eth does not return anything, even after running setup.exe).

0 件の賞賛
返信

769件の閲覧回数
addiyi
NXP Employee
NXP Employee

Try several times the ccs command findcc cwtaps -eth. There was an issue in ccs (I think in your ccs version it is present) where the ccs is not able to discover all the devices from network.

 

Are the cwtap and your pc in the same sub-network?

Adrian

0 件の賞賛
返信

769件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rodney McLendon,

1. Please check whether CDDE path is valid in Hardware configuration manager window, for example <Installation path>\eclipse\Optimization\target-connection\cdde\cdde-windows\bin\cdde.exe.

2. In the CCS console, please enter the following commands and check the result.

(bin) 7 % config cc cwtap:10.15.146.9
(bin) 8 % show cc
CodeWarrior TAP Boot Loader version 1.0.1
CodeWarrior TAP OS version 1.0.1

3. Do you have a valid DDRv license deployed in <INSTALL_DIR>\eclipse\ProcessorExpert\?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信