QCVS Component Start Address Won't Change

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS Component Start Address Won't Change

1,556件の閲覧回数
rodneymclendon
Contributor I

How do I change the QCVS component start address?

 

169659_169659.pngpastedImage_2.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,422件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rodney McLendon ,

This value is configured by the system automatically.

For the DDR less than 2G the start address is configured as 0x0, for DDR larger than 2G, it is configured as 0x10000000.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,422件の閲覧回数
addiyi
NXP Employee
NXP Employee

QCVS assumes that LAW for first DDR region is set starting with 0x0 and have 2Gbytes in size. To be able to change the start address you should use a size at most 2Gbytes.

Adrian

0 件の賞賛
返信