Programming/Debugging of MCF5282

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming/Debugging of MCF5282

7,209 Views
TTA
Contributor I
Hi,
 
I would like to know if JTAG and BDM are available on the MCF5282, and if both these interfaces can be used to program the internal flash memory on a bare board (which does not contain any downloader/firmware)
 
How can we program the internal flash on a new board , and what hw/sw will be required for this purpose?
 
 
Labels (1)
0 Kudos
Reply
4 Replies

2,909 Views
marc_paquette
Contributor V
According to Freescale's product summary, the MCF5282 has JTAG and BDM:
 
 
Consult this PDF for information about programming the on-board flash memory:
 
 
If you have more questions, let me know.
 
Marc.
0 Kudos
Reply

2,908 Views
TTA
Contributor I
The cyclone Max allows us to program via BDM. It does not mention programming flash/ram via JTAG.

Can we write to the internal flash directly using the Cyclone Max? Or do we need to use a loader program in the SRAM first, and then load the image to the Flash?

TTA

Message Edited by TTA on 02-27-200610:08 AM

0 Kudos
Reply

2,908 Views
marc_paquette
Contributor V
CodeWarrior Dev Studio for ColdFire 6.2 allows you to program the on-chip flash memory using any supported hardware connection (examples: P&E Microcomputer's USB and parallel devices, Abatron's BDI1000 and BDI2000 devices):
 
 
CodeWarrior tools for ColdFire currently do not support P&E's Cyclone Max, but I've passed your message along as a feature request.
 
To get more information about Cyclone Max, please contact P&E directly:
 
 
Marc.
0 Kudos
Reply

2,908 Views
TTA
Contributor I
hi marc.

thanks a lot!

So my options for bareboard programming are:

BDI2000 + codewarrior ( listed as supported )

or, PE CycloneMAX + the tools provided by them.

TTA
0 Kudos
Reply