Problem with Codewarrior USB TAP: mpc603e: Core not responding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Codewarrior USB TAP: mpc603e: Core not responding

2,703件の閲覧回数
Orchen
Contributor I

Hi,

I have installed CW 8.8. But Failed when I  connect MPC8241 with USB TAP(debug->attach the process),the error message is "CCSProtocolplugin::Could not connect the requested core core #0".

but I connect MPC8548 and MPC8313 successfully with USB TAP. 

Can someone help me?

 

log:

CCS: 0000    :    ccs_open
CCS:        :        ipaddr = 127.0.0.1
CCS:        :        port = 41475
CCS:        :        timeout = 10
CCS:        :        serverh = 0
CCS:        :    ccs_open; ccs_error = 0
CCS: 0000    :    ccs_get_connection_count
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_get_connection_count; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 0
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 0
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_config_cc
CCS:        :        serverh = 0
CCS:        :        config_string = utap:0
CCS:        :    ccs_config_cc; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_set_timeout
CCS:        :        serverh = 0
CCS:        :        timeout = 10
CCS:        :    ccs_set_timeout; ccs_error = 0
CCS: 0000    :    ccs_config_server
CCS:        :        serverh = 0
CCS:        :        cc = 0
CCS:        :        server_config = 0
CCS:        :        value = 782
CCS:        :    ccs_config_server; ccs_error = 0
CCS: 0000    :    ccs_get_config_chain
CCS:        :        serverh = 0
CCS:        :        device_list: (size = 0)
CCS:        :    ccs_get_config_chain; ccs_error = 0
CCS: 0000    :    ccs_config_chain
CCS:        :        serverh = 0
CCS:        :        cc = 0
CCS:        :        device_list: (size = 1)
CCS:        :            device[0]:: core_type=31;    device_descr=[ir_length:0;dr_bypass_length:0;bypass_instruction:0]
CCS:        :    ccs_config_chain; ccs_error = 39
CCS:        :        Error message:
mpc603e: Core not responding

CCS: 0000    :    ccs_delete_cc
CCS:        :        serverh = 0
CCS:        :        count = 0
CCS:        :    ccs_delete_cc; ccs_error = 0
CCS: 0000    :    ccs_close
CCS:        :        serverh = 0
CCS:        :    ccs_close; ccs_error = 0

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,536件の閲覧回数
J2MEJediMaster
Specialist I

Have you installed the latest v 8.8.3 patch for CodeWarrior? It is available here on the Power Architecture CodeWarrior Updates page.

 

---Tom

0 件の賞賛
返信