Problem when enabling tracing and profiling for the P3041DS board -- No matching command converters.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem when enabling tracing and profiling for the P3041DS board -- No matching command converters.

ソリューションへジャンプ
6,856件の閲覧回数
samehsamir
Contributor I

Hello,

 

I'm trying to enable tracing in a CodeWarrior debug session. I've succeeded in debugging the Linux kernel as illustrated in the CodeWarrior for Power Architecture targeting manual via a CodeWarrior TAP in attach mode

(i.e., Stop U-boot from autobooting, Attach from CodeWarrior, boot from U-boot prompt).

 

When enabling the "Start a trace session" checkbox from within the debug configuration, the following error shows.

 

Failed to configure plugin Trace Probe - NPC.

 

The function "applyConfig" returned an error condition  (0x80004005)

Error from TCF: 2147500037 (Did not find matching command converter. Present command converters: cc: 0 cwtap:0)

 

19640_19640.pngsnapshot2.png

19641_19641.pngsnapshot3.png

It also happens when using a DDR buffer for tracing instead of an NPC buffer. I am running CodeWarrior from a 64-bit Ubuntu 12.04 installation.

 

Thank you,

Sameh

ラベル(1)
0 件の賞賛
返信
1 解決策
6,459件の閲覧回数
addiyi
NXP Employee
NXP Employee

Workaround for this kind of issue, when the probe used is CodeWarrior TAP is to use Connection Type: CodeWarrior TAP with Hardware connection: Ethernet, or to use Connection type: USB TAP.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
15 返答(返信)
6,460件の閲覧回数
addiyi
NXP Employee
NXP Employee

Workaround for this kind of issue, when the probe used is CodeWarrior TAP is to use Connection Type: CodeWarrior TAP with Hardware connection: Ethernet, or to use Connection type: USB TAP.

Adrian

0 件の賞賛
返信
6,459件の閲覧回数
addiyi
NXP Employee
NXP Employee

I'm using CodeWarrior for PA 10.4.0 and I was able to collect trace using a cwtap and a stationary project. Please try to use stationary project and Download configuration to see if the issue is reproducible.

Adrian

0 件の賞賛
返信
6,459件の閲覧回数
samehsamir
Contributor I

I created a bareboard application -- not sure if that is what you mean by a stationary project -- for P3041 and copied code from the e500mcPerformanceMonitor_eabi sample project. Debugging works fine for both the Download and Cache Download debug configurations, but when enabling tracing the previous error still happens.

Thank you,

Sameh

0 件の賞賛
返信
6,459件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please try only with the default bareboard project. From the Wizard select Download launch and Start a trace session on debug launch. After you start the debug session using Download configuration, and application stops a main, click Resume and trace should be collected.

Adrian

0 件の賞賛
返信
6,459件の閲覧回数
samehsamir
Contributor I

I tried the default bareboard project with all the settings you mentioned. The error persists. The only setting I had to modify for debugging was the JTAG clock speed from the target settings. The following error message is shown:

Error launching p3041-core00_RAM_P3041_Download

CCSProtocolPlugin : Failed to configure the JTAG chain. Simulator/CCS is already configured to use a JTAG Chain different than the target type specified in CodeWarrior debugger settings

[CCS last error: Connection refused ]

The default clock speed chosen is 10230 kHz. In the drop down menu, only 4000kHz and 12500kHz are shown. Picking any option from them bypasses this error, but tracing is still not enabled. I also changed this setting in previous projects.

Thank you,

Sameh

0 件の賞賛
返信
6,459件の閲覧回数
addiyi
NXP Employee
NXP Employee

OK, so you are able to enter debug, program stop at main and after Resume you receive errors? Usually after Resume, you can find Trace data in Software Analysis view.

Adrian

0 件の賞賛
返信
6,459件の閲覧回数
samehsamir
Contributor I

I see the same original error. Even after pressing OK and cancelling exporting of diagnostics, there is no trace data in the Software analysis window.

snapshot5.png

This problem also occurs on CodeWarrior 10.4.0 installed on Windows 7 (Evaluation version).

0 件の賞賛
返信
6,459件の閲覧回数
addiyi
NXP Employee
NXP Employee

For CCS server, did you use Automatic launch or Manual launch? Also, if Manual launch is used, CCS server is opened remote?

Adrian

0 件の賞賛
返信
6,459件の閲覧回数
samehsamir
Contributor I

Automatic launch was configured for CCS server.

Thanks,

Sameh

0 件の賞賛
返信
6,460件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi Sameh,

Could you please provide a recent log from /home/<user>/.codewarrior

Adrian

0 件の賞賛
返信
6,460件の閲覧回数
samehsamir
Contributor I

Hello Adrian,

Here's the contents of codewarrior.log after this error:

08:08:08.322 WARN  [0xc1089b40] sae.deapi_utils      : [parseDeapiConfigFileLine]: line <> does not have expected format
08:08:08.323 WARN  [0xc1089b40] sae.deapi_utils      : [parseDeapiConfigFileLine]: line <> does not have expected format
08:08:08.343 WARN  [0xbb07cb40] tcf.peer             : Failed connecting to remote peer
08:08:08.346 WARN  [0xbb07cb40] tcf.peer             : Failed connecting to remote peer
08:08:08.397 WARN  [0xbb07cb40] tcf.peer             : Failed connecting to remote peer

Thank you,

Sameh

0 件の賞賛
返信
6,460件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi Sameh,

The log say nothing about the issue. Let's try to set the logger to debug mode:

1. Rename /home/<user>/.codewarrior/ log4cxx.xml.temp to log4cxx.xml

2. Edit the xml file and set the verbosity to debug if is not already set:

<root>

<priority value="debug"/>

<appender-ref ref="CodewarriorAppender" />

</root>

3. Reproduce the issue again and send the log file.

Adrian

0 件の賞賛
返信
6,460件の閲覧回数
samehsamir
Contributor I

Hi Adrian,

The logs are a bit large and I don't have the capability/privilege to upload files. I will send it to you via email.

Thanks,

Sameh

0 件の賞賛
返信
6,460件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please indicate the CodeWarrior version you are using.

Adrian

0 件の賞賛
返信
6,460件の閲覧回数
samehsamir
Contributor I

I am using the latest CodeWarrior v10.4 for Power Architecture, with the Linux service pack 1 and e500mc toolchain.

Thank you,

Sameh

0 件の賞賛
返信