Problem in licesing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in licesing

1,268 Views
VinothLC
Contributor I

When i run the code warrior development suite which is of  FLOATING subscription, after installing the license file, it tells some error with the license file carrying the status as ' Unable to find key from

Win32_PLUGINS_PPCCPU_NOT FIND THE HOST' .

 

It also says waiting for background operation.

 

Please provide help in this.

 

Thanks,

 

Vinoth

Labels (1)
0 Kudos
Reply
1 Reply

1,125 Views
J2MEJediMaster
Specialist I

A couple of questions:

 

1) Is the FLEXlm licensing software set up properly on the server? For more information, go to this web page and follow the Vendor Daemons link.

 

2) The licensing software comunicates on certain TCP ports in order to function. This requires that these ports be open (unblocked). Your network administrator needs to ensure that the firewall is not blocking these ports.

 

3) Even though your network adminstrator says the ports are unblocked, insist that he do it. Nine out of ten floating-license problems, from my experience, are because to these critical ports being blocked, even though the IT person says that they aren't. The licensing software can generate a log that can help you spot problems with the network.

 

---Tom

0 Kudos
Reply